Basic work bench for collaborative applications
EX-01238Collaboration right at the bench – the basic work bench as an entry into the world of collaborative work benches. In this way, both the worker and the robot arm have full access to the entire working area. The working height can be set to an ergonomic level using four height-adjustable Lifting Columns. There is plenty of space below the bench to fit the control system. The size of the table top can be selected according to the work involved.
Note: A collaborative mode of operation is essential in the case of work bench systems. Stability must be checked in line with the scale of the solution and robot model.